Team,
Can you please help with register and jumper/sw configuration for interfacing PCM3070 with CC2564 on USBMODEVM?
the specifics are that
CC2564 doesnt output MCLK (so we use SW2 to configure MCLK to come from USB)
CC2564 output 44.1 16bit I2S with BCLK and LRCLK
From the PCM3070-KCS we could load the first script (high performance playback), and just from switching the I2S source with SW2 we could hear distorted sound on line out corresponding to the stream sent to the CC2564.
I suggested customer to play with BLCK setting so that it would become the only reference to the DACs and set a proper values in the clock/pll tab corresponding to 44.1KHz. But it doesnt improve anything.
can you please suggest what modifications from high performance playback script should be do to configure the part properly?
olivier