This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question Abotu TAS5760 Bootstrap Cap

Genius 4220 points
Other Parts Discussed in Thread: TAS5704, TAS5760XXEVM

Hi,

There isn't any info about the capacitance value and voltage rating for the bootstrap capacitor.

I found the 0.22uF/25V cera cap is used for the TAS5760EVM and TAS5704EVM.

so. the following description in TAS5704 D/S can be applied to TAS5760, right?

"The half H-bridge output stages use only NMOS transistors. Therefore, they require bootstrap capacitors for

thehigh side of each output to turn on correctly. A 220-nF ceramic capacitor, rated for at least 25 V, must be

connected from each output to its corresponding bootstrap input."

Thanks,

Go