This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Digital input PORTA/B sync on SRC4392

Quick question:

I have an external I2S digital source (BCLK, WCLK, DATA) connected to the PORTB input. I am trying to redirect this data to the SRC, and then SRC ouput to the DIT but I can't manage to make it work.

Do the digital inputs PORTA and PORTB have to be synchronized with the MCLK when configured as inputs?

Thanks !

  • Hi, Thierry,

    Welcome to e2e, and thanks for your interest in our products!

    This is discussed in the data sheet in the section titled, "MASTER AND REFERENCE CLOCKS" on page 24, and also in the section titled, "AUDIO SERIAL PORT OPERATION" on page 25.

    -d2