Other Parts Discussed in Thread: TAS5630B, TAS5624A, TAS5630
Hello,
I was looking into the possibility of making a single PCB for TAS5630B and be able to use it as 4 x SE, 2 x BTL or 2 x SE + 1 x BTL channels.
One way would be to stuff/ unstuff components and change the mode settings accordingly.
Can I hardwire the amplifier as 4 x SE and use any two channels as BTL by giving out of phase signal inputs to those channels? Will the dc bias given in SE mode cancel out when used with another channel configured in SE mode? Will such a connection be recommended?
If yes, what needs to be the output inductor value when used as BTL o/p?
Thanks in advance and regards,
Ravindra.