Other Parts Discussed in Thread: CC8520
Greetings E2@.
Please advise on the following questions.
- We are only using one channel. It seems that I can select 5Mbps signaling and Protocol B in this situation. Will that provide enough robustness that we will get good results with the minimum buffer size (640 samples)? That would provide acceptable latency. If not, what buffer size do we realistically need for good robustness?
- It seems like the CC8520 chipset may be somewhat "soft" (firmware driven), and that the Configurator may load the firmware into the chip. If that is the case, is there any possibility of getting a "special" firmware version that would improve the latency for our particular application: PCME24, single channel, single slave?
On another track, can you tell me if TI might have any new products on the horizon that would be a better fit for our application? In addition to lower latency (< 10 ms desired), we would prefer a larger number of independent "networks" to be possible--at least 6 to 10. Also bit-accurate 20 or 24 bits would be preferred.
regards
Madhuri