This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2707C problem?

hello:

I have two questions:

(1) PCM2707C is connected for an I2S-enabled application, When HID0/MS is pulled up,the inner DAC is stoped, can I2S continue work?

(2) The input clock frequency is 12Mhz, but the sampling rate of most music is 44.1kHz, for better performance, if the input clock frequency can configure as 11.2896Mhz? How does the clock work?