This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2001D1 / Output power in TA=-20~60℃

Guru 29720 points
Other Parts Discussed in Thread: TPA2001D1, TPA2010D1, TPA2011D1
Hi,
 
My customer concerns if TPA2001D1 is capable of 1W output in Ta=-20~60℃.
The datasheet shows 1W(TYP) in Ta=25℃ only, so I believe it is incapable.
Is my understanding correct?
Could you please give me your advice about this inquiry?
 
Best Regards,
Yaita
  • Hi, Yaita-san,

    This is a VERY old device. I suggest you look at one of our newer devices like TPA2010D1 or TPA2011D1.

    To answer your question, the device's output power is limited by the power dissipation and junction temperature rise. You need to calculate the power dissipation and then use the thermal resistance to calculate the junction temperature. If it's below 150C, then you are ok, if it exceeds 150C, then you will trip the thermal protection.

    -d2

  • Hi Don-san,
     
    Thank you for your suggestion.
    I will recommend the newer device as you mentioned.
     
    By the way, how do I estimate power dissipation of TPA2001D1?
    I aplologize for basic question...however, is it possible to estimate from a certain value in datasheet?
     
    Best regards,
    Yaita
  • Hi Don-san,
     
    I heard supply current of TPA2001D1 is 320mA@5V when 1W output(RL=8Ω, TA=25℃) from my customer.
    So, I try to estimate if TPA2001D1 can output 1W in TA=60℃ as following. 
     
    Pd=Ps-Po
        =(320mA x 5V) - 1W
        =600mW ------(1)
    -----------------------------
    Pd: power dissipation
    Ps: supply power 
    Po: output power
    -----------------------------
     
    According to datasheet, dissipation rating of TA=60℃ is 557mW ------(2)
    *774mW - {(60℃ - 25℃) x 6.19mW/℃}=557mW
     
     
    It seems (1)>(2), so I think TPA2001D1 can't output 1W in TA=60℃.
    Is my understanding correct?
     
    Best Regards,
    Yaita
  • Don-san,
     
    Is my calculation process correct?
     
    Best Regards,
    Yaita
  • Hi, Yaita-san,

    Yes, it looks correct to me.

    -d2

  • Hi Don-san,
     
    Thank you for your confirming.
    I appreciate for your support.
     
    Best Regards,
    Yaita