Hi! :)
I have built the amp using TAS5630 chip. I have found in my prototype that the idle output noise level depends on the supply voltage (PVDD). The higher is the PVDD, the lower is the output noise. Is it typical for this chip? I am using PVDD=35V now, and the output noise is a little bit too high for me. I can hear it from the loudspeaker in the distance about 20-30 centimeters. I have developed my own PCB layout design, very similar to the reference design from TI, using a solid ground plane too. The noise seems to be not in the result of EMI, because I can touch any output switching node before LC filters, and the noise level stays the same. I have tried to insert some additional ceramic caps in various places with no any change also.
I know the clock generator in class-D amp can be the source of the noise too, so does it makes a sence to use some high quality low noise crystall oscillator together with TAS5630? I can run it in slave mode and connect the powered XTAL generator to the OSC+/- pins. Will this help? Or the source of the noise is something other?
Many thanks and best regards,
Alex