Hello,
I recently received an evaluation kit for PCM1865 DAC to be evaluated for our upcoming product.
Problem is that I can't seem to connect to EVM correctly using Purepath console.
PPC reports that device is not connected, and Windows device manager reports this device as "unknown", and therefore is unable to find proper driver for it.
Purepath console is latest version downloaded today. (7/22/14)
This leads me to wonder, that there is an issue with the USB-I2X board delivered with EVM. To further analyze problem I connected the EVM to linux computer which reported:
idVendor=ffff
idProduct=fffe
This is clearly not correct.
I am using Windows 8.1 pro 64bit system, to use purepath console and EVM.
EVM itself was bought from Mouser Electronics, if this helps tracing the problem.
br,
Tapio