Dear community,
LM48580 maximum power dissipation numbers in datasheet is given for 6uF buzzer capacity.
How can I calculate power dissipation, if I use buzzer with much smaller (8-11nF) capacity? Can I estimate, that it could be few hundreds times lower, than shown on Figure 12 in datasheet?
Also, how could I estimate power consumption at frequencies, higher than 200Hz? Figure 12 shows very high values even for 2kHz, but I suspect that my system could produce sound with much higher frequencies, up to 10kHz.
Output voltage generated is 25Vpp.