Hi there,
I am thinking of using a class-D stereo speaker amp to drive two 4ohm 2W (normal) speakers. Just wondering the current need for the power supply for the speaker VDD. Do we calculate for the max current or the average current when using the power supply for the speaker VDD?
Assuming that I have to drive the 4ohm 2W speakers, and my speaker VDD is at 5V, I have (5V*0.707)^2/4ohm * 0.85(efficiency of the class D amp)=2.65W delivered to each of the speaker. Now this calculation is based on a pure sine wave. What if the wave form is such that a maximum load is reached? And how do I spec for the power supply? how much current should the supply provide?
thanks,
TC