I am moving a design with a AIC3204 from single ended to differential input and used the configuration recommended in the data sheet, i.e. routing the positive and negative input to the amplifier via a 10kohm resistor. The inputs are capacitively coupled (as in figure 5-1 in the datasheet) but I can measure that I have no DC bias at the input pins (it gets the bias from the DC leakage in my coupling capacitors – which are ”unstable” and gives problems).
Shall I also use common mode on the input amplifers, i.e. change page 1 register 54 (left MICPGA negative terminal) from 0x10 (IN2R with 10kohm) to 0xD0 (IN2R with 10kohm and CM with 40kohm)?
Or shall I use page 1 register 58 and weakly connect all inputs to common mode?
BR
Søren