Hello again,
This evaluation board seems to be getting more and more problematic. As described in our earlier discussion on this product, I did receive a faulty evaluation kit, which has been replaced by Mouser.
Old discussion: http://e2e.ti.com/support/data_converters/audio_converters/f/64/p/356716/1252690.aspx#1252690
The new board seemed promising at the start (at least it was recognized correctly by PC and USB-Lock led was lit), but either the Purepath console software or the PCM1865 itself is acting weirdly.
I have tried running console program in all kinds of compatibility and administration modes, but no effect on funtionality.
The exact problem here is that there seems to be no I2C connectivity to PCM1865 whatsoever. The configuration on EVM is as described in EVM user guide pdf. Meaning that there is jumpers J8 and J11 present on board.
When I try to read registers using "Registers" tab on purepath console software, the software just hangs for something like 20seconds and then returns nothing at all. (See screenshot below)
Also it tried connecting an oscilloscope to SDA and SCL pins on EVM board. There is a large burst of I2C traffic, when USB cable is first connected, but this stops afterwards. When I open "Registers" tab or click refresh on said tab, there is some traffic visible, but it is just address call, which repeats every 15ms. Below is zoomed picture of such burst:
What can be seen from this figure is that I2C bus does not receive an ACK pulse from slave, which is done by pulling SDA down during pulse number 9. This means, that master decides that the slave is not present and does not do anything else for it.
This made me wonder that PCM communication mode is wrong, or address pin is pulled high or something, so I added jumpers from MD0 and MD1 to ground to ensure, that they are configured correctly. This had no effect whatsoever.
-Tapio