Hello,
I have two questions:
1. Figure 13 of the TAS5717 datasheet shows the output power vs. supply voltage characteristics of the chip. The note says that the dotted line represents the thermally limited region. I don't really understand this graph. Does it mean that I cannot use a 16V supply voltage to drive my 10W speakers?
2. All the graphs (including and especially Figure 13) are always shown with an 8 ohms load. However, the specs seem to allow a 4 ohms load. How will the THD behave at 4 ohms?
Kind regards,
~ Joel Bodenmann