Other Parts Discussed in Thread: TPA3122D2, PCM1865, PCM1863, PCM1861, PCM9211
Here is what I am trying to do... Convert an audio signal to a PWM signal, invert and buffer this signal so it can be sent to a remote location using unshielded twisted pair cabling, then at the remote location have a power stage to drive a loudspeaker. I was thinking of using something like the tpa3122d2 to generate the PWM signal, but I'm not so sure it will work correctly for this application... as it will have no real load applied to it. Does the tpa3122d2 require a load to correctly adjust the PWM output? Is there something designed to provide a pwm output without the power stage that would be better suited to this purpose? Any suggestions as to a power buffer I could use to drive the speakers? they will be 4ohm and looking at something in the 10 - 30 watt range