This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
My client intends to use TAS5711 as single filter PBTL like attached schematic..
However, there are big POP when PWM had ON ( 0x05= 00) ( wave form attached.
blue and light-blue is each ouput) ,
Following is the register-setting. It seems no problem..
~~~~~~~~~~~~~~~~~client's setting from~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
! Factory Trim
X1b 00
! wait 25ms
! PBTL setting
X20 00 01 77 72
X25 01 00 22 45
X19 3A
! PWM On
X05 00
~~~~~~~~~~~~~~~~~~~~~~to here~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
Question 1
The BST cap in EVM ( C16,C22, C45, C9) are 33nF in EVM, but client use 3.3nF.
What range of should be used for BST cap's value. ( ex at least 10nF...)
Question2
If PBTL pin were High,TAS5711 automatically set PWM_A = PWM_B, PWM_C=PWM_D ?
If so, I think 0x25=01 00 22 45 (client's setting: PWM1=A=B,PWM3=C=D ) and
also 01 10 32 45 ( data sheet p34 PWM1=B,PWM2=A, PWM4=C,PWM3=D) is both OK in case
0x19=3A (PWM2 and PWM4= shutdown).
Is it correct?
Question 3
I think TAS5711 work under single filter PBTL, but you mentioned TAS5727 is fine in
another post. (*) Would you please let me know the reason?
(*)
http://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6/t/97585.aspx
I hope your answer wtihin2 days
Thank you nad with my best regards
Hello Shibatani,
I will try to post a response later today once I reviewed your post and questions.
Shibatani,
Damian,
In PBTL does BSTA need to be connected to BSTB, and BSTC need to be connected to BSTD? I know this is a requirement for the TAS5731M, but I see no reference to this on the TAS5711? I would assume that the BST pins need to be synchronous for all paralleled output stages.
Thanks,
Adam
Hi Adam,
This isn't a requirement for TAS5711 as for TAS5731M. This is requirement based on the output power design, which is different for the two devices.