This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254EVM-U as USB class audio device + WinCE 7



Good morning/day/evening/night.

There are:

ARM-based data terminal (Waysion X7);

TLV320AIC3254EVM-U.

I want to connect it between itselves and work with EVM as with USB class audio device. X7's OS - WinCE 7. As EVM was being connected with X7, it lighted LED like it was working, but audio streaming still continued onto onboard speakers. 

Is it possible to work with this EVM as with usb class audio device on WinCE7?

Can i set the sampling rate of mic/line inputs up to 192 kHz and how?

-hiv