When using the TLV320AIC3204, and if the ADC input is overdriven ( IN1_L/R) > .5VRMS, distortion/noise feeds through to the digital output drive for the speaker. Is this expected behavior and is there is a way to configure the part to eliminate this effect?
I don't believe I'm exceeding the Absolute Maximum Voltage on those pins from the table in the data sheet but If I am it is a momentary transient. I think it takes just a little more that .5VRMS.