Hi, we're getting close to final layout and have a few questions:The TAS5756M has the DAC output exposed for feeding back into the amplifier via an external ac-coupling capacitor, but it may be desired to use the line-out directly as well as the amp. Does the TAS5756M have the same line driver as the 512x part where you can simply hook it up directly to the line output connector via external RC network? If this network is used for filtering out of band noise on the 512x, what is different in the 5756 that doesn't require this network? Is it internal prior to the DAC out pins?Would you recommend buffering the DAC output if using it to drive line outputs as well as feed back into the amplifier?Also, we noted that page4 of data sheet has "headphone amp" listed - an error we assume?Also, if we were to add a headphone amp (we're considering the tpa6133a as we already use this elsewhere) how would you recommend we do so based on the above line out questions?