Greetings,
We are using the TLV320AIC3204 in an audio recorder. Record/playback is great. But, during setup/record when the user has headphones plugged in, there is a delay through the headphones, which gives the user a really annoying echo (of the live sound plus the delayed sound in headphones). Any registers that can be tickled to control this?
Here is the current register configuration:
page0 | ||
[0] | 0x0000 | Page Select Register |
[1] | 0x0000 | Software Reset Register |
[2] | 0x0060 | Reserved Register |
[3] | 0x0000 | Reserved Register |
[4] | 0x0000 | Clock Setting Register 1, Multiplexers |
[5] | 0x0011 | Clock Setting Register 2, PLL P&R Values |
[6] | 0x0004 | Clock Setting Register 3, PLL J Values |
[7] | 0x0000 | Clock Setting Register 4, PLL D Values (MSB) |
[8] | 0x0000 | Clock Setting Register 5, PLL D Values (LSB) |
[9] | 0x0000 | Reserved Register |
[10] | 0x0000 | Reserved Register |
[11] | 0x0081 | Clock Setting Register 6, NDAC Values |
[12] | 0x0082 | Clock Setting Register 7, MDAC Values |
[13] | 0x0000 | DAC OSR Setting Register 1, MSB Value |
[14] | 0x0080 | DAC OSR Setting Register 2, LSB Value |
[15] | 0x0002 | Reserved Register |
[16] | 0x0000 | Reserved Register |
[17] | 0x0008 | Reserved Register |
[18] | 0x0081 | Clock Setting Register 8, NADC Values |
[19] | 0x0082 | Clock Setting Register 9, MADC Values |
[20] | 0x0080 | ADC Oversampling (AOSR) Register |
[21] | 0x0001 | Reserved Register |
[22] | 0x0000 | Reserved Register |
[23] | 0x0004 | Reserved Register |
[24] | 0x0000 | Reserved Register |
[25] | 0x0000 | Clock Setting Register 10, Multiplexers |
[26] | 0x0001 | Clock Setting Register 11, CLKOUT M divider value |
[27] | 0x000D | Audio Interface Setting Register 1 |
[28] | 0x0000 | Audio Interface Setting Register 2, Data offset setting |
[29] | 0x0000 | Audio Interface Setting Register 3 |
[30] | 0x0088 | Clock Setting Register 12, BCLK N Divider |
[31] | 0x0000 | Audio Interface Setting Register 4, Secondary Audio Interface |
[32] | 0x0000 | Audio Interface Setting Register 5 |
[33] | 0x0000 | Audio Interface Setting Register 6 |
[34] | 0x0000 | Digital Interface Misc. Setting Register |
[35] | 0x0000 | Reserved Register |
[36] | 0x00CC | ADC Flag Register |
[37] | 0x00AA | DAC Flag Register 1 |
[38] | 0x0011 | DAC Flag Register 2 |
[39] | 0x0000 | Reserved Register |
[40] | 0x0000 | Reserved Register |
[41] | 0x0000 | Reserved Register |
[42] | 0x0000 | Sticky Flag Register 1 |
[43] | 0x0000 | Interrupt Flag Register 1 |
[44] | 0x00C0 | Sticky Flag Register 2 |
[45] | 0x0000 | Sticky Flag Register 3 |
[46] | 0x00C0 | Interrupt Flag Register 2 |
[47] | 0x0000 | Interrupt Flag Register 3 |
[48] | 0x0000 | INT1 Interrupt Control Register |
[49] | 0x0000 | INT2 Interrupt Control Register |
[50] | 0x0000 | Reserved Register |
[51] | 0x0000 | Reserved Register |
[52] | 0x0000 | GPIO/MFP5 Control Register |
[53] | 0x0012 | DOUT/MFP2 Function Control Register |
[54] | 0x0002 | DIN/MFP1 Function Control Register |
[55] | 0x0002 | MISO/MFP4 Function Control Register |
[56] | 0x0002 | SCLK/MFP3 Function Control Register |
[57] | 0x0000 | Reserved Registers |
[58] | 0x0000 | Reserved Registers |
[59] | 0x0000 | Reserved Registers |
[60] | 0x0001 | DAC Signal Processing Block Control Register |
[61] | 0x0001 | ADC Signal Processing Block Control Register |
[62] | 0x0000 | Reserved Register |
[63] | 0x00D4 | DAC Channel Setup Register 1 |
[64] | 0x0002 | DAC Channel Setup Register 2 |
[65] | 0x0000 | Left DAC Channel Digital Volume Control Register |
[66] | 0x0000 | Right DAC Channel Digital Volume Control Register |
[67] | 0x0000 | Headset Detection Configuration Register |
[68] | 0x006F | DRC Control Register 1 |
[69] | 0x0038 | DRC Control Register 2 |
[70] | 0x0000 | DRC Control Register 3 |
[71] | 0x0000 | Beep Generator Register 1 |
[72] | 0x0000 | Beep Generator Register 2 |
[73] | 0x0000 | Beep Generator Register 3 |
[74] | 0x0000 | Beep Generator Register 4 |
[75] | 0x00EE | Beep Generator Register 5 |
[76] | 0x0010 | Beep Generator Register 6 |
[77] | 0x00D8 | Beep Generator Register 7 |
[78] | 0x007E | Beep Generator Register 8 |
[79] | 0x00E3 | Beep Generator Register 9 |
[80] | 0x0000 | Reserved Register |
[81] | 0x00C0 | ADC Channel Setup Register |
[82] | 0x0000 | ADC Fine Gain Adjust Register |
[83] | 0x0000 | Left ADC Channel Volume Control Register |
[84] | 0x0000 | Right ADC Channel Volume Control Register |
[85] | 0x0000 | ADC Phase Adjust Register |
[86] | 0x0000 | Left Channel AGC Control Register 1 |
[87] | 0x0000 | Left Channel AGC Control Register 2 |
[88] | 0x007F | Left Channel AGC Control Register 3 |
[89] | 0x0000 | Left Channel AGC Control Register 4 |
[90] | 0x0000 | Left Channel AGC Control Register 5 |
[91] | 0x0000 | Left Channel AGC Control Register 6 |
[92] | 0x0000 | Left Channel AGC Control Register 7 |
[93] | 0x0000 | Left Channel AGC Control Register 8 |
[94] | 0x0000 | Right Channel AGC Control Register 1 |
[95] | 0x0000 | Right Channel AGC Control Register 2 |
[96] | 0x007F | Right Channel AGC Control Register 3 |
[97] | 0x0000 | Right Channel AGC Control Register 4 |
[98] | 0x0000 | Right Channel AGC Control Register 5 |
[99] | 0x0000 | Right Channel AGC Control Register 6 |
[100] | 0x0000 | Right Channel AGC Control Register 7 |
[101] | 0x0000 | Right Channel AGC Control Register 8 |
[102] | 0x0000 | DC Measurement Register 1 |
[103] | 0x0000 | DC Measurement Register 2 |
[104] | 0x0000 | Left Channel DC Measurement Output Register 1 |
[105] | 0x0000 | Left Channel DC Measurement Output Register 2 |
[106] | 0x0000 | Left Channel DC Measurement Output Register 3 |
[107] | 0x0000 | Right Channel DC Measurement Output Register 1 |
[108] | 0x0000 | Right Channel DC Measurement Output Register 2 |
[109] | 0x0000 | Right Channel DC Measurement Output Register 3 |
[110] | 0x0000 | Reserved Register |
[111] | 0x0000 | Reserved Register |
[112] | 0x0000 | Reserved Register |
[113] | 0x0000 | Reserved Register |
[114] | 0x0000 | Reserved Register |
[115] | 0x0000 | Reserved Register |
[116] | 0x0000 | Reserved Register |
[117] | 0x0000 | Reserved Register |
[118] | 0x0000 | Reserved Register |
[119] | 0x0000 | Reserved Register |
[120] | 0x0000 | Reserved Register |
[121] | 0x0000 | Reserved Register |
[122] | 0x0000 | Reserved Register |
[123] | 0x0000 | Reserved Register |
[124] | 0x0000 | Reserved Register |
[125] | 0x0000 | Reserved Register |
[126] | 0x0000 | Reserved Register |
[127] | 0x0000 | Reserved Register |
page1 | ||
[0] | 0x0001 | Page Select Register |
[1] | 0x0008 | Power Configuration Register |
[2] | 0x0001 | LDO Control Register |
[3] | 0x0000 | Playback Configuration Register 1 |
[4] | 0x0000 | Playback Configuration Register 2 |
[5] | 0x0000 | Reserved Register |
[6] | 0x0000 | Reserved Register |
[7] | 0x0000 | Reserved Register |
[8] | 0x0000 | Reserved Register |
[9] | 0x0030 | Output Driver Power Control Register |
[10] | 0x0000 | Common Mode Control Register |
[11] | 0x0010 | Over Current Protection Configuration Register |
[12] | 0x0008 | HPL Routing Selection Register |
[13] | 0x0008 | HPR Routing Selection Register |
[14] | 0x0000 | LOL Routing Selection Register |
[15] | 0x0000 | LOR Routing Selection Register |
[16] | 0x0000 | HPL Driver Gain Setting Register |
[17] | 0x0000 | HPR Driver Gain Setting Register |
[18] | 0x0040 | LOL Driver Gain Setting Register |
[19] | 0x0040 | LOR Driver Gain Setting Register |
[20] | 0x0000 | Headphone Driver Startup Control Register |
[21] | 0x0000 | Reserved Register |
[22] | 0x0000 | IN1L to HPL Volume Control Register |
[23] | 0x0000 | IN1R to HPR Volume Control Register |
[24] | 0x0000 | Mixer Amplifier Left Volume Control Register |
[25] | 0x0000 | Mixer Amplifier Right Volume Control Register |
[26] | 0x0000 | Reserved Register |
[27] | 0x0000 | Reserved Register |
[28] | 0x0000 | Reserved Register |
[29] | 0x0000 | Reserved Register |
[30] | 0x0000 | Reserved Register |
[31] | 0x0000 | Reserved Register |
[32] | 0x0000 | Reserved Register |
[33] | 0x0000 | Reserved Register |
[34] | 0x0000 | Reserved Register |
[35] | 0x0000 | Reserved Register |
[36] | 0x0000 | Reserved Register |
[37] | 0x0000 | Reserved Register |
[38] | 0x0000 | Reserved Register |
[39] | 0x0000 | Reserved Register |
[40] | 0x0000 | Reserved Register |
[41] | 0x0000 | Reserved Register |
[42] | 0x0000 | Reserved Register |
[43] | 0x0000 | Reserved Register |
[44] | 0x0000 | Reserved Register |
[45] | 0x0000 | Reserved Register |
[46] | 0x0000 | Reserved Register |
[47] | 0x0000 | Reserved Register |
[48] | 0x0000 | Reserved Register |
[49] | 0x0000 | Reserved Register |
[50] | 0x0000 | Reserved Register |
[51] | 0x0040 | MICBIAS Configuration Register |
[52] | 0x0080 | Left MICPGA Positive Terminal Input Routing Configuration Register |
[53] | 0x0000 | Reserved Register |
[54] | 0x0080 | Left MICPGA Negative Terminal Input Routing Configuration Register |
[55] | 0x0080 | Right MICPGA Positive Terminal Input Routing Configuration Register |
[56] | 0x0000 | Reserved Register |
[57] | 0x0080 | Right MICPGA Negative Terminal Input Routing Configuration Register |
[58] | 0x0000 | Floating Input Configuration Register |
[59] | 0x000C | Left MICPGA Volume Control Register |
[60] | 0x000C | Right MICPGA Volume Control Register |
[61] | 0x0000 | ADC Power Tune Configuration Register |
[62] | 0x0003 | ADC Analog Volume Control Flag Register |
[63] | 0x00C0 | DAC Analog Gain Control Flag Register |
[64] | 0x0000 | Reserved Register |
[65] | 0x0000 | Reserved Register |
[66] | 0x0000 | Reserved Register |
[67] | 0x0000 | Reserved Register |
[68] | 0x0000 | Reserved Register |
[69] | 0x0000 | Reserved Register |
[70] | 0x0000 | Reserved Register |
[71] | 0x0000 | Analog Input Quick Charging Configuration Register |
[72] | 0x0000 | Reserved Register |
[73] | 0x0000 | Reserved Register |
[74] | 0x0000 | Reserved Register |
[75] | 0x0000 | Reserved Register |
[76] | 0x0000 | Reserved Register |
[77] | 0x0000 | Reserved Register |
[78] | 0x0000 | Reserved Register |
[79] | 0x0000 | Reserved Register |
[80] | 0x0000 | Reserved Register |
[81] | 0x0000 | Reserved Register |
[82] | 0x0000 | Reserved Register |
[83] | 0x0000 | Reserved Register |
[84] | 0x0000 | Reserved Register |
[85] | 0x0000 | Reserved Register |
[86] | 0x0000 | Reserved Register |
[87] | 0x0000 | Reserved Register |
[88] | 0x0000 | Reserved Register |
[89] | 0x0000 | Reserved Register |
[90] | 0x0000 | Reserved Register |
[91] | 0x0000 | Reserved Register |
[92] | 0x0000 | Reserved Register |
[93] | 0x0000 | Reserved Register |
[94] | 0x0000 | Reserved Register |
[95] | 0x0000 | Reserved Register |
[96] | 0x0000 | Reserved Register |
[97] | 0x0000 | Reserved Register |
[98] | 0x0000 | Reserved Register |
[99] | 0x0000 | Reserved Register |
[100] | 0x0000 | Reserved Register |
[101] | 0x0000 | Reserved Register |
[102] | 0x0000 | Reserved Register |
[103] | 0x0000 | Reserved Register |
[104] | 0x0000 | Reserved Register |
[105] | 0x0000 | Reserved Register |
[106] | 0x0000 | Reserved Register |
[107] | 0x0000 | Reserved Register |
[108] | 0x0000 | Reserved Register |
[109] | 0x0000 | Reserved Register |
[110] | 0x0000 | Reserved Register |
[111] | 0x0000 | Reserved Register |
[112] | 0x0000 | Reserved Register |
[113] | 0x0000 | Reserved Register |
[114] | 0x0000 | Reserved Register |
[115] | 0x0000 | Reserved Register |
[116] | 0x0000 | Reserved Register |
[117] | 0x0000 | Reserved Register |
[118] | 0x0000 | Reserved Register |
[119] | 0x0000 | Reserved Register |
[120] | 0x0000 | Reserved Register |
[121] | 0x0000 | Reserved Register |
[122] | 0x0000 | Reserved Register |
[123] | 0x0005 | Reference Power-up Configuration Register |
[124] | 0x0000 | Reserved Register |
[125] | 0x0000 | Reserved Register |
[126] | 0x0000 | Reserved Register |
[127] | 0x0000 | Reserved Register |