This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC3101 Settings

Other Parts Discussed in Thread: TLV320ADC3101

Good Day,

I have some questions about the configuration of the TLV320ADC3101. We are using Processing Block 1 (PRB_R1). In the datasheet (Figure 31) it is mentioned that the condition MADCxAOSR >= IADC must be met. Is IADC (Page 0 /Register 21) configurable when using PRB_R1 or is it fixed to 188 as shown in table 6 in the datasheet?! Is the decimation ration (Page 0/Register 22) freely configurable for PRB_R1?!

Thanks and have a nice day

Marc