I'm am working on a simple self-powered (not bus-powered) USB DAC using the PCM2707. While it functions correctly, I am getting a noticeable thump both when the USB is connected or disconnected and on power up/power down. Monitoring the outputs with a scope shows DC offset is the cause. The circuit, specifically the output filter and DC blocking capacitors, matches the datasheet and EVM for the PCM2707. Any idea on why this could be occurring?
Thanks for your help!
Andrew