Hi there,
I just trying to configure an 2+1 wireless system using CC8530 with 4ch ADC on the transmitter side and 4ch DAC on the receiver side. I have already working the transmitter configured like that:
front/primary left channel on [ AD0 / LEFT / PCM16 ]
front/primary right channel on [ AD0 / RIGHT / PCM16 ]
subwoofer channel on [ AD1 / LEFT / PCM16 ]
Can I configure the receiving CC8530 in this same way, to receive with a single CC8530 all the 3 PCM16 streams? I cannot find the option in PurePath Wireless Configurator... there are just mono/stereo options for receiver...
Thanx,
Tomasz