A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: PCM3070Hello Community!
I`ve been building an Digital Sound processor with our PCM3070.
I had allready programmed a Software, with can read an write sucessfully from the Chip.
Also i`ve tested this Configuration for the PCM on this post(PGA Anaog Bypass): http://e2e.ti.com/support/data_converters/audio_converters/f/64/t/270914.aspx
It works!
I can hear the IN1_L R signal on the HP_L R.
So my question: in which way can i send the complete configuration file to my PCM3070?
If it is necessary for you, i would do an pre-pre amp Application.
Our PCM should do the input Volume control, the equalizer, maybe a Filter. Also the chip has to do the routing of the 3 inputs to the output of the chip.
thanx a lot!
iam from Germany!
here is the scematic for the board, on which is the PCM3070 adapted.
Jumper 4 must be closed, if i want to hear sommething while the Code from the upper post is loaded.