Looking for some concrete numbers regarding settling time and conversion speed for the PCM1754 audio DAC. I have some system requirements constraints and need to be sure I'm meeting them.
Does TI have a number for the full scale settling time of this chip? Since it's not in the datasheet, I am trying to derive it based on system clock specs, serial data setup and hold time, oversampling considerations, etc. But it would be nice to have a real number from TI on this. Based on 200 kHz max sample rate, one could say settling time is less than 5 usec, but it should be much faster than that.