This is from page 37 of the TAS5756M datasheet. What is the "MCLK CMOS oscillator source" referring to? Is there a crystal oscillator on the chip which would let me directly hook a crystal up to it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
This is from page 37 of the TAS5756M datasheet. What is the "MCLK CMOS oscillator source" referring to? Is there a crystal oscillator on the chip which would let me directly hook a crystal up to it?
Hello Jon,
It means that you can provide an external 3.3V (CMOS level) clock to TAS5756M MCLK pin (e.g. 24.567MHz) and use the internal PLL dividers to generate the SCLK (also known as bit clock) and LRCLK (also known as frame sync clock).