Other Parts Discussed in Thread: TAS5421-Q1
In Datasheet fot TAS5421-Q1
DC Detect—This circuit checks for a dc offset continuously during normal operation at the output of the amplifier. If a dc offset occurs, the device asserts the FAULT pin and updates the I2C register. Note that the dc detection threshold follows PVDD changes.
What happends if Vehicle voltage (8-32 V) will be shorted to speaker output?
It will occur bit "In a fault condition" in Status and Load Diagnostic Register (0x02)?
What does it mean "Note that the dc detection threshold follows PVDD changes"?
As i understand SpeakerGuard needed for protect speaker.
How it affect on Status and Load Diagnostic Register?
What happends if Vehicle voltage (8-32 V) will be shorted to speaker output, if I set in Control Register (0x03) bit for "SpeakerGuard protection circuitry set to 5.9-V peak output". Something changes versus SpeakerGuard turned off?
Will speaker output going to Hi-Z state In this case?
Will amplifier working properly after Vehicle voltage will disappear on speaker outputs?
What voltage can appear on PVDD in this case? If PVDD may rise, then how much it can be?