Other Parts Discussed in Thread: PCM3168, PCM4204
Hi...
I previously worked with PCM3168 using the differential buffers shown in PCM4204 datasheet...
Now i want to use the buffers presented in the PCM3168 datasheet, mainly cause of a size problem (the other buffers are to big).
My question is if VCOMAD/DA should be buffered to each input/output buffer, as it's done in the PCM4204 buffer, or can i simply connect VCOM to V+ pin of my OpAmp used in the buffer? i'm not sure if i made my question clear....
Another question... In the PCM3168 datasheet, for differential input, is shown a circuit made only of resistors and capacitors, with no buffer... As i'm trying to do the PCB the smalles possible, this kind of input is tempting me... What problems would use this circuits? i assume impedance copuling would be the problem... am i right?