Other Parts Discussed in Thread: PCM1794, PCM5102A
If IG1&IG2 is DAC Chip PCM1794 Iout(+&-)(RorL),can I replace the feedback capacitor C8&C9&C3 to 100pF or more lesser value?
Beacuse I want let almost no phase shift at 20Hz-22KHz .
C8=C9=C3=2700pF IG1 to VM1 phase
C8=C9=C3=100pF IG1 to VM1 phase
but i'm not understand have any other effect. DAC Chip will fine?
The Datasheet of PCM1794 page.20 used 2200pF&2700pF to let fc=217KHz,why? (if analog output to LPF>speaker,theres no human ear can hear)(The LPF or speaker hardware burnt by >217KHz signal?)
The PCM1794 pin (Iout+&-|L&R) should no output signal at user select sampling rate(more high frequency signal),so even can removal feedback capacitor?
sorry about my poor english