I have read " AN-1849 An Audio Amplifier Power Supply Design " and it says that the transformer used is dual primary and secondary transformer of 300VA and output 24 volts. but the design says the rail voltages are +/- 72V. the design uses 2 transformers and in the schematic each transformer's dual secondary outputs are connected in series which will make the output go to +/- 48 volts. I need to know if i'm wrong and what is the correct explanation regarding my understanding, if i'm wrong.