We are installing a product in our helicopters that uses the LM4862 Audio amplifier for an alert warning to the pilots.
We are connecting multiple outputs(including the LM4862 output) of varying voltage levels to a single input using isolation resistors.
When only one product is supplying an audio warning at a time, this causes a voltage to be seen at the inactive LM4862 outputs.
What is the reverse breakdown voltage of the LM4862 outputs so that we do not damage the products?