Other Parts Discussed in Thread: TAS5631B
Hello,
My customer is using TAS5631B for their new product ( ES ) and evaluating.
Please let me know about Rocp for TAS5631B.
In the TAS5631B data sheet SLES263C,
Rocp is 22Kohm to 33Kohm in case C by C mode. for PHD package. and also
Rocp is 47Kohm to 64Kohm in case latching mode .
Here is the question
Q1
I can see if 47Kohm was set, then Ioc=15Atyp for latching mode in D/S page 10 . But, how about another value (from 47K to 64Kohm.)?
What is the meaing of the range between 47K to 64K?
My understanding is , Even though Rocp was set to 64Kohm, Ioc= 15A, is it correct ?
Q2
Customer choosed Rocp=39Kohm .... the information from china OEM and cutomer don't know the reason.
Do you recommend Rocp= 39Kohm?
Can you guess the background?
Customer is designing the next stage ( pilot run ) and it is in hurry.
Please let me know withind 2days..
With My Best Regards