Dear Sir \ Madam
I am designing an audio product with the OPA1632 as an audio ADC front end connected as single ended to differential converter.
My requirement is as follow :
input signal level 3.6V P/P output signal level 2.4V P/P operating voltage +/-15V ,VCOM buffered and drive from the ADC and set to 2.5V (P/P = peak to peak)
and required input impedance is 47Kohm.
My problem is with the required input impedance.
I have try to use TI application note "Fully-Differential Amplifiers SLOA054D" to design the Amplifier but the required input impedance want fit into the formulas provided.
My design schematic is similar to the schematic showed in the application section of the OPA1632 data sheet.
Please help
Thank you
Yuval