Hello! Could you please show me the output frequency responce? I look for this information in datasheet but there is no figure about.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello! Could you please show me the output frequency responce? I look for this information in datasheet but there is no figure about.
The attached pdf shows the frequency response using the TAS2552 EVM:
VBAT = 5V
Boost on
Load = 8Ohm + 33uH
AUX-0025 analog filter on APx525 balanced inputs
20kHZ LP AES17 filter on APx525
no weighting
0dBFS
15dB PGA gain
48kHz sampling rate
digital input