This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Nicolas,
For AIC3105 with MCLK of 12MHZ and a desired DAC/ADC sampling frequency of 8KHz, first you need to have a proper sampling frequency for the codec (48KHz).
If MCLK is 12MHz, then you need to enable PLL and set their values as follows:
Then, in order to achieve an exact sampling frequency of 8KHz in DAC and ADC, you need to set NDAC and NADC with a value of 6 (48KHz / 6 = 8KHz). this is set in Codec Sample Rate Select Register (Page 0/Register 2).
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hello Nicolas,
If you are using TLV320AIC3105EVM with USBMODEVM, the MCLK signal generated from the motherboard has an approximated frequency of 11.28MHz. If you configure the device with the given values, the ADC and DAC sampling frequency will be close to 7.5KHz. If you want to achieve the 8KHz sampling frequency with the EVM, you need to use an external MCLK or change the values of the PLL constants.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer