This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AIC3254 BCLK jitter implications in voice mono

I am going to use a AIC3254 in slave mode controlling from FPGA:

MCLK,BCLK,WCLK.

BCLK output from FPGA should have low jitter: 100ps cycle to cycle rms or less. 

1/

What are the implications if the constraint below is not met.

2/

do you know if that constraint can be "released" for voice application (8Khz mono)

and if yes how much this can be ?

 

  • Hello,

    The device is designed to withstand 100ps of jitter as you mentioned. If the jitter is a bit higher than that, you will start seeing skirts in FFTs which gets worse with input frequency as well as distortion components. If it is much more than that you will start getting audible noise artifacts.

    Regards,

    J-