This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI communication endurance



Hello I had a quick question on the read/write endurance of the SPI on the CC85XX

..Lets just say I didn't have an interrupt line to a host controller from a CC85XX, and because of that had to poll the SPI status word diligently in order to see if any network events/datagrams had occured.  and I planned on doing this ~8 Hz.  Do I have to worry about read/write endurance, or is it some sort of ram and it shouldn't be a problem?  

Half the reason is because of limited pins on my specific uC and the other half is because the current boards do not have this provision and I would like to use these for a short run of long-term prototypes.  Ideally I will include this feature in future revisions, but I am not curious if I would be wearing out something on the CC85xx by implementing this for production products.

Thank you,

Zack