I am using two LM4950 on a board powered by same main source power supply. These amps are in a high gain mode but the signals cross talk quiet a bit. I have seprate ground and power back to the source. The supply for one is going through a linear regulator. I was wondering why is there a cross talk. Moreover is there an active circuit solution to reduce cross talk. I need to be 75 db down. I though PSRR etc would help me out but that is not the case. I need some suggestion or guidance to an active circuit to reduce this problem.