Hi everyone
I Cant seem to get this device to work, I have gone over the data sheet several times and don't seem to be getting anywhere
I have used one of the PCM1803a breakout boards that are available, mainly to see how it will work before I go as far as making up PCBs.
I have set FMT0 and FMT1 to 5v and the same with MOD0 and Mod1, this should have set the device as master with a right justified 20 bit data
the breakout board has a 2.56mhz oscillator feeding SCK (pin 15).
As the device is set in master I assumed that once powered up with an analog input on VINL and VINR I would have at least clock signals from BCK or LRCK but I have absolutely nothing.
I have 2 of these boards and it is the exact same with both,