This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204 Biquad coefficients

Other Parts Discussed in Thread: COEFFICIENT-CALC

I am trying to use the Matlab FDAtool to generate IIR filter coefieficients.  I am a bit confused as to the format of the data.

 

 

 

Numerator Section 1 = 1, -1.706681886025, 1

Denominator Section 1 = 1, -1.527217053584, 0.7184480476664

Numerator section 2  = 1, 0.4714206650502, 1

Denominator section 2 = 1, -0.7855219502704, 0.1828606950272

Numerator section 3 = 1, -1.844088863607, 1

Denominator section 3 = 1, -1.826943294536, 0.9574809532943

Numerator section 4 = 1, -1.355793289995, 1

Denominator section 4 = 1, -1.198817610676, 0.4794199882168

Numerator section 5 = 1, -1.810111156144, 1

Denominator section 5 = 1, -1.714882124594, 0.8614509371445

I tried multipying the numbers by (2^23-1 )and then scaling them by 6 dB or in other words multiplying them by (2^22-1) to prevent an overflow.  My question is do I have to divide the N1 and D1 by two and negate D1 and D2 based on the equation in the data sheet (5.1).

 

Any way I tried two scenarioios and neither one seems to work.

 

 

 

 

 

 

Int16 BiquadCoeff[50] = {

 

//ChebyII 10th order 5 section biquad 022210 from Jeff Solum

 

 

//Section 1

0x3F,0xFFFF, 0xC9,0x62DD, 0x3F,0xFFFF, 0xCF,0x210A, 0x2D,0xFB0E,

 

 

//Section 2

0x3F,0xFFFF, 0x0F,0x15E0, 0x3F,0xFFFF, 0xE6,0xDD02, 0x0B,0xB3FD,

 

 

//Section 3

0x3F,0xFFFF, 0xC4,0xFD39, 0x3F,0xFFFF, 0xC5,0x89AF, 0x3D,0x475E,

 

 

//Section 4

0x3F,0xFFFF, 0xD4,0x9D57, 0x3F,0xFFFF, 0xD9,0xA34A, 0x1E,0xAED1,

 

 

//Section 5

0x3F,0xFFFF, 0xC6,0x1392, 0x3F,0xFFFF, 0xC9,0x1FC0, 0x37,0x2203,

};

/*Int16 BiquadCoeff[50] = { //ChebyII 10th order 5 section biquad 022210 from Jeff Solum with signs changed on D1 and D2

//Section 1

0x3F,0xFFFF, 0xC9,0x62DD, 0x3F,0xFFFF, 0x30,0xDEF6, 0xD2,0x04F2,

//Section 2

0x3F,0xFFFF, 0x0F,0x15E0, 0x3F,0xFFFF, 0x19,0x22FE, 0xF4,0x4C03,

//Section 3

0x3F,0xFFFF, 0xC4,0xFD39, 0x3F,0xFFFF, 0x3A,0x7651, 0xC2,0xB8A2,

//Section 4

0x3F,0xFFFF, 0xD4,0x9D57, 0x3F,0xFFFF, 0x26,0x5CB6, 0xE1,0x512F,

//Section 5

0x3F,0xFFFF, 0xC6,0x1392, 0x3F,0xFFFF, 0x36,0xE040, 0xC8,0xDDFD,

};*/