I am developing a system using the TLV320AIC3104 CODEC, which has an AGC module I am not using. Is it possible to use the AGC to estimate and output the strength of a line-in signal, without it affecting gain in the PGA? I am wondering if I can set up the AGC to compute the gain it would like to apply, which I could read from the AGC gain registers (32 and 33), and which then gives me a measure of the line in signal strength.