Hi all,
I want to setup TAS5756M using TDM Mode offset N input
3 wire(SLCK, SCLK & Data) setup is using
where
LRCK/FS = 48kHz
SLCK = 4.608MHz (96bit per sample
The audio is ok when (P0-R41)offset = 0x01,0x31,0x21
The audio is not ok when (P0-R41)offset = 0x51
May I know if TAS5756 support the input format (or if 128bit per sample is required in TDM mode?)
Or if there is any limit when setting the (P0-R41)offset register?
Here list related register I'm setting
P0-R20 0x02
P0-R21 0x20
P0-R22 0x00
P0-R23 0x00
P0-R24 0x01
P0-R27 0x01
P0-R28 0x0F
P0-R29 0x03
P0-R30 0x07
P0-R34 0x00
P0-R35 0x04
P0-R36 0x00
P0-R40 0x10
P0-R41 0x51
P0-R42 0x01
Raymond Fu