Other Parts Discussed in Thread: TAS5708, TAS5709, TAS5707
Hello,
I've tried to set the DRC with the following settings:
gain: 0 (O = 0.064516 = 0x00084210)
threshold: -64 (T = 14.616484 = 0x074ee8f0)
ratio 30:1 (k = -0.966667 = 0x03844445)
attack, release and energy to 100ms (a<x>: 0.000227 = 0x0000076d)(1 - a<x>: 0x007ff892
The only thing responding is the gain. Although it applies the gain no matter the setting of the DRC CONTROL register.
I've tried to get register settings from various EVM GUI tools to verify my calculations but they all crash when pressing the 'Time Constants' button in the DRC Customisation tool or won't install at all.
Can someone supply me with working register values so I can see if my calculations are off or that the problem lies somewhere else? Is there another setting I'm missing to enable the DRC besides D0 in the DRC Control register?
With kind regards,
Allex Veldman