Other Parts Discussed in Thread: TPA3106D1, TPA3100D2
Hello,
I am working on a design using two TPA3106D1 amplifiers as a stereo pair. I have a few items that I would like to clear up:
1) Since I am using one unit as the master, do I need ROSC stuffed on the slave unit? If not, what should I do with the pin?
2) Any special considerations for VREG between the two chips?
3) Is it OK to directly control SHUTDOWN and MUTE direcly from a microcontroller pin/digital VCC? Or would it be better to buffer through a transistor and use VREG?
Any other hints/considerations outside the data sheets/app notes would be greatly appreciated!
Thanks,
JP