Hi
I am looking for a suitable audio codec with high enough sampling rate. In the above series I find that there are two main versions of the chips, one with 96kHz and the other series with 192kHz sampling rate. This is advertised on the website as well as the starting page of the data sheet. However digging further into the data sheet only discusses setting sampling rates of 48kHz and lower. No where does it say how to set 96kHz or a non standard sampling rate.
Is the advertised maximum sampling rate there to pull in people but cannot really be set or used even if settable?
Please clarify.
Thanks
Manjula