Other Parts Discussed in Thread: TAS2505, AM3352
Hi Sir,
Do we have Linux driver for TAS2505?
Customer(WNA) are using TAS2505 with AM3352 and they could not find a driver code on SDK8.0.
Thanks,
Patrick
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Patrick,
We don't have a Linux driver for this device. TAS2505 is a device controlled via I2C, so technically there is no driver for this device. You need to use a master device (AM3352 for your application) and send the I2C commands to the device. I would suggest creating a script with the help of the amplifier GUI and then load it into the device.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer