Other Parts Discussed in Thread: PCM5310, PCM3168
Hello,
I am looking at using a PCM5310 codec in place of a current system that uses an AD1938 codec. I require three ADCs and 2 DACs. An ADAU1446 DSP is configured as master and the system has no on-board uC. Given the numerous registers that can be configured on the PCM5310, is it even possible to use it without a uC? I simply want to pass the three ADC channels to the DSP and then pass two channels of audio from the DSP to the DACs. This is quite simple to implement with the AD1938 codec, but it is very costly.
Thanks,
ACW