Hi!
My application requires THD to be < 1%.
Based on the datasheet for the TPA6130A2 (Figures 3 through 6), the tested gains are 0.1 dB and 6.1 dB. The 6.1 dB plots are only for BTL though.
What is the maximum Gain with THD < 1 % for RL=16 ohms Stereo configuration at 100mW?
I am concerned that increasing the Gain to 4dB would affect the THD performance at 100mW. When I look at the 16 ohm stereo plot below it shows good THD performance at 100 mW out, but it specifies a gain of 0.1dB.
If the THD would still be below 1% at 100mW out with 4 dB gain through the amp, I would use that gain. It would also allow me to reduce the required input swing of the amp by a factor of 1.58 (i.e. I would only need a swing of 2.3Vpp at the amp input if the THD performance is still good at 4 dB of gain). Does that make sense?
Thanks for your help in advance!!
James