This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about TAS5766M Coefficient data.

Guru 19685 points

I read TAS766M Coefficient data 3 times.

It was different (change) in a data of following Page-Address.

------------------------------------------------------------

Page44                   read 1    read 2    read 3

 Address:20h     4A   5A   21

 Address:21h     20   80   C0

Page45

 Address:08h     CC   C2   CC

 Address:09h     E0   00   E0

Page52

 Address:1Ch     00   02   01

 Address:1Dh     96   8F   5A

 Address:1Eh     79   C5   63

Page70

 Address:60h     4A   5A   21

 Address:61h     20   80   C0

※There were no changes for other coefficient data.

------------------------------------------------------------

Please let me know about two point below.

・What are the contents of these Page-Addess?

 I think that page 44(20h/21h) and page 45(08h/09h) are the Biquad filters.

 but, i didn't find information of page 52(1Ch/1Dh/1Eh) and page 70(60h/61h).

・As stated above, these coefficient data were change, is it no problem?

 

Best regards,

Satoshi

  • Hi Satoshi-san,

    Some of the C-RAM locations are written by the miniDSP algorithm itself. Changes to the C-RAM locations below are expected from dump to dump:

    C6   Page 0x2C, Register 0x20
    C7   Page 0x2C, Register 0x24
    C30  Page 0x2D, Register 0x08
    C31  Page 0x2D, Register 0x0C
    C32  Page 0x2D, Register 0x10
    C37  Page 0x2D, Register 0x24
    C38  Page 0x2D, Register 0x28
    C39  Page 0x2D, Register 0x2C
    C53  Page 0x2D, Register 0x64
    C54  Page 0x2D, Register 0x68
    C59  Page 0x2D, Register 0x7C
    C93  Page 0x2F, Register 0x14
    C245 Page 0x34, Register 0x1C

    Regards,

    Jorge

  • Dear Jorge-san

    Thank you for reply.

    Is Change in Page-70(0x46) also OK?

    Best regards,
    Satoshi
  • Hi Satoshi,

    Yes. That would be C245 in Buffer B. See updated list below.

    C6   Page 0x2C/0x3E, Register 0x20
    C7   Page 0x2C/0x3E, Register 0x24
    C30  Page 0x2D/0x3F, Register 0x08
    C31  Page 0x2D/0x3F, Register 0x0C
    C32  Page 0x2D/0x3F, Register 0x10
    C37  Page 0x2D/0x3F, Register 0x24
    C38  Page 0x2D/0x3F, Register 0x28
    C39  Page 0x2D/0x3F, Register 0x2C
    C53  Page 0x2D/0x3F, Register 0x64
    C54  Page 0x2D/0x3F, Register 0x68
    C59  Page 0x2D/0x3F, Register 0x7C
    C93  Page 0x2F/0x41, Register 0x14
    C245 Page 0x34/0x46, Register 0x1C

    Regards,

    Jorge

  • Note that Page 70, Register 0x60 is Reserved and not part of C-RAM. The last coefficient is C255 which is on Pages 0x2C/0x46, Registers 0x44-0x47.