Other Parts Discussed in Thread: CC8531
Hi,
I work on a project using PurePath technology (chip CC8531).
For our needs, the product must work either as a master or as a slave.
The “PurePath Wireless Configurator” allows to configure a firmware and program it.
But we then have a static configuration inside the product.
Is it possible to program a firmware which can be dynamically configured (using host control) in master or slave ?
Same question for bidirectional/downstream/upstream.
If it is not possible, I have to envisage a bigger memory in my microcontroller in order to store multiple configurations.
But the other issue is that the number or write/erase cycles for the flash of CC8531 is limited to 1000 (cf cc8531.pdf).
It is low according the number of switch that we would have in the product.
What do you recommend ?